Part Number: HD3SS6126
Hi,
HD3SS6126 this USB3.0 and USB2.0 one-two switch chip, USB3.0 interface can be used as USB2.0?
Can this chip be used as a three-way USB2.0 switch?

Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
You can not use the HD3SS6126 SuperSpeed Signal for USB2.0 signaling since its max Viop-p is only 1.8V while USB2.0 can go up to 3.3V.

When you say three-way USB2.0 switch, do you mean 1 to 3 MUX?
Thanks
David
Hi,
I will go ahead and close this thread due to inactivity, you can respond back to re-open this thread if you have any update.
Thanks
David