This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: LED_x pin configuration for blinking external LED

Part Number: DP83867IR

Hello team,


Our customer is considering to use DP83867IR.

Then, they'd like to make the circuit which can confirm 100BASE-TX/1000BASE-T link status by external LED using LED_x pin.
Also, they want to use LED_x pin as strap configuration as well.

Then, could you provide suggested circuit for this application using 3.3V power supply for LED and controlling transistor by LED_x pin out put when VDDIO is 1.8V?(It is same as datasheet p55)

Also, below is their configuration.

  1. LEDCR1 and LEDCR2 is default
  2. LED_x pin mode config are as below
    1. LED_0 : mode1
    2. LED_1 : mode4
    3. LED_2 : mode1

If possible, it is really helpful is you provide resistor divider setting which can achieve above setting at DP83867ERGZ EVM users guide's LED_STRAP PINS.

Also, could you please tell me LED_1/2 status(Hi-Z or Lo) when 100/100BT is unlinked?
We understood there is PD but we'd like to know about the output logic circuit status.

Best regards,
Kazuki Kuramochi