Part Number: TUSB320HA
Other Parts Discussed in Thread: TUSB320
Dear Sirs and Madams,
We are considering the TUSB320 and would like to confirm for the voltage on the CC pin.
I understand that the datasheet specs are as follows:

How should we consider the conditions of "0.61V or more and less than 0.7V" and "1.16V or more and less than 1.31V"?
Although the USB standard specifies a threshold value, the TUSB320 data sheet does not include a threshold value, so I asked this question.
(1)
Does TUSB320 have similar thresholds as the USB specification?
Or are these voltage range of this device "undefined"?

(2)
I understand that it is an "Unattached State (OUT1 and OUT2 are 'H')" when it is less than 0.25V, but is that correct?
Or does it need to be less than 0.2V, which is the USB specification threshold or 0.15V of max voltage?

Regards,
MM