Part Number: SN75DPHY440SS
The total length from Video source to sink is 600 mm, so I intend to put a re-driver in the middle.
The source Video data is MIPI CSI-2 v1.3 configured to use D-PHY v1.2, 1 or 2 lanes. The maximum bit rate is 1.5 Gbps/Lane.
From the DPHY440SS data sheet: The DPHY440SS is a one to four lane and clock MIPI DPHY re-driver that regenerates the DPHY signalling. The device complies with MIPI DPHY 1.1 standard and can be used in either a MIPI CSI-2 or MIPI DSI application at data rates of up to 1.5 Gbps.
Does it matter that the SN75DPHY440SS is MIPI DPHY 1.1 rather than 1.2?
Under what conditions will it work or fail?
There does not appear to be an equivalent DPHY 1.2 compliant version of SN75DPHY440SS - is there another IC that would do the re-driver job?
Thanks for your assistance.