Part Number: DS125DF410
Tool/software:
Hi,Ti-team
Please tell me about register address 0x33.
[Question]
1. Is it correct to understand that this register is enabled when ADAPT_MODE is set to “11”?
2. Both HEO and VEO are 4-bit settings and the default value is 8, but what is the unit of this register?
3. For example, if the input eye pattern aperture is ±0.1UI and there is a signal with a lot of jitter,
is it better to change the HEO_THRESH setting from the default value of 8 to 15 so that it can be locked?
Regards,