This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1050: Standard compliance with ISO 11898-1 and ISO 11898-2.

Part Number: SN65HVD1050
Other Parts Discussed in Thread: TCAN1057A-Q1

Tool/software:

Hi Team

Hope you are doing well,

I want to use SN65HVD1050DR  Ic for my project,

for that i want to know that whether this IC(SN65HVD1050DR)  will comply with ISO 11898-1 and ISO 11898-2.

 Thanks & Regards 

Ujjwal

  • Hi Ujjjwal,

     The device is comply with ISO 11898-2 which is physical layer requirement of CAN. ISO 11898-1 is the data link definition, it's not necessarily relevant to the CAN transceiver.

    And we don't recommend to use SN65HVD1050 for new designs, please migrate to TCAN1057A-Q1 with upgraded performance and even lower price.

    Regards,

    Sean