Part Number: TCAN1051HGV
Tool/software:
Hello Team,
We're currently using TCAN1051HGVDR in our custom board where the schematic component is different from the actual part used. The component in the schematics is for TCAN1051HGDR and the required part is TCAN1051HGVDR. The pin 5 is a NC pin in schematics which is not connected but its the Vio pin which is responsible for the voltage level of cantx and rx pin. Since nothing is connected in pin 5, the chip isn't working.

To confirm the working of this, we tried to give 3.3v to the pin 5 with a jumper and the chip worked.
With 5 V supply and 3.3V IO compatible, is there a possible part which can be replaced instead of TCAN1051HGVDR without the schematics being modified as the custom board is already manufactured.
The above requirement might look irrelevant, but if there is a solution for this then that should be very helpful
Thanks in advance.