This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV32E: Need clarification on allowable input voltage

Part Number: AM26LV32E

Tool/software:

Could someone please clarify for me whether the AM26LV32E's 1A/B, 2A/B, 3A/B, 4A/B inputs can accept a 5V signal (with the supply set to 3.3V)?

The datasheet has this note:

"Accepts 5-V logic inputs with 3.3-V supply (enable inputs)"

Which leads me to believe that the 1-4A/B inputs can NOT accept 5V input, only the G/G' can accept 5V input.

Thanks!