This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: ON TX port bonding of DS90UB954

Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: TIGER

Tool/software:

Dear Sir,

For example, RX0  port  is mapping to TX0,  RX1  is mapping to TX1, is it workable?

Thanks! 

  • Hello Tiger,

    the UB954 can be used either in 4-lanes at one TX mode where you can use it for any or both RX inputs. Or you can use it with 2-lanes at two TX mode where you can use it for replication only. Means you cannot RX0 to TX0, RX1 to TX1.

    If you want each RX input to be mapped to one TX output, then you should use the UB960.