Tool/software:
hi expert,
There is a question about the 4G or 2G POC circuit of DS90UB960.
The DS90UB960 is used in the Headunit. It is to communicate with camera module.The serializer is DS90UB933 in the camera module.
The POC circuit is designed to power camera module . There are two kinds of POC circuits in the DS90UB960 spec. One is 4G,another one is 2G.
Refer to the below picture, it is the 4G POC circuit in the Head unit.The POC circuit of Camera module is the 2G structure.
Question:
Can the DS90UB960 with 4G POC and the DS90UB933 with 2G POC work together?
Please let me know if you need more information?