This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIC12400-Q1: IN_STAT_COMP can be latched?

Part Number: TIC12400-Q1

Tool/software:

Hello team,

There is a usage situation, MCU need to check the source/channel after being waked up, checking the datasheet, the IN_STAT_COMP can report individual channel states, but it cannot be latched until read, for example, if a switch was pushed and released, the IN_STAT_COMP will record nothing, and MCU can only be waked but miss the source.

The /INT scheme can only latch INT_STAT register and /INT pin, but cannot specify which channel, so do you have any suggestions for the requirement?

Thanks

Regards,

Daniel Wang