This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320LAI: I2C bus design inquiry

Part Number: TUSB320LAI

Tool/software:

Hi team,

In the following TUSB320LAI datasheet note that, if I2C is pull up to 3.3V, VDD need to be 3.0V and above.

Customer now I2C pull up voltage is1.8V,  since our TUSB320LAI VDD power supply range is 2.7V ~5V, does it OK for them to keep I2C 1.8V pull up work while VDD power supply is off?

Does the 1.8V I2C pull up voltage get risk to back power the device?

Regards,

Will