This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5013-Q1: Thermal cut-out

Part Number: LM5013-Q1

Tool/software:

Hi,

I'm having issues with the LM5013-Q1 going into thermal shutdown well below the design current of 3.2A. It shuts down after 54 seconds from 30C ambient at a continuous 2A.

I read elsewhere that the Vin and Ground pins require a reasonable amount of copper to transfer heat. Granted my layout hasn't accounted for this, but I'm dubious as to weather improving those copper areas will allow stable operation at 3.2A. I tried soldering some heavy copper wire to the Vin area between C66 & C67 to try and improve thermal dissipation but the time to thermal shutdown from ambient was only improved by 6 seconds (1 minute). This may well just be coincidental anyway.

Here's my schematic:



Here is the layout. PCB is a two layer, top and bottom copper pours are 0V/ground.