Other Parts Discussed in Thread: ALP, DS90UB960-Q1, DS90UB933-Q1
Tool/software:
Hi
遇到个问题,我尝试了单独使用DS90UB960-Q1 EVM时,软件使用正常,且能识别到SER的型号,但是,当通过DS90UB960-Q1 EVM,Mini-Fakra 连接上DS90UB933 -Q1 EVM时,ALP软件就使用卡顿了,且软件不能识别出ser和des的型号
Tool/software:
Hi
遇到个问题,我尝试了单独使用DS90UB960-Q1 EVM时,软件使用正常,且能识别到SER的型号,但是,当通过DS90UB960-Q1 EVM,Mini-Fakra 连接上DS90UB933 -Q1 EVM时,ALP软件就使用卡顿了,且软件不能识别出ser和des的型号
Part Number: DS90UB960-Q1EVM
Tool/software:
Hi all
please below question and hope you can give help ,thank you
1. when connect the J37 of DS90UB960-Q1 EVM to desktop by using micro-USB cable, i can know the Device Information in Analog LaunchPAD software
2. but when i using the mini-Fakra cable ( it is support PoC ,right?) connect to the DS90UB933-Q1 EVM, i can't get any information in LPD tool, even 960 information
i attach the image of connected for yours, is it any else i need setup ?
Looking forward to your early reply,thank you
Hello Gong,
Yes, the 960 supports PoC and it seems there are no issues with the jumper settings.
What is the power rating of the power supply that you are using to power the 960 EVM? Since the power supply will power 2 PCBs, maybe the power supply is not able to supply enough power.
Can you ensure the power supply is at least 12V/1A?
Best,
Justin Phan