This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: Output lines not being pulled to VccA voltage

Part Number: LSF0108

Tool/software:

Dear Team,

I am using LSF0108QWRKSRQ1 and i have also attached a snapshot.
In this VccB i have used as 3.3V and VccA as  1.8V mentioned as Vadj FMC.
The HPD from the TX connector is given as 3.3V on VccB side when i measure, but after the level translator it is giving 2.7V instead 1.8V.

Regards,
Irfan