Part Number: TCA9511A
Other Parts Discussed in Thread: INA236, , TCA9803, ISO1643
Hi team!
1.Could you please tell me whether the TCA95711 really recognizes low level at 0.3*Vcc?
2. I would like to use the INA236 to communicate with an isolator whose VOL is 0.6 to 0.8V.
Will this be possible if I use the TCA9511A?
In other words:
Isolator <-> TCA9511A <-> INA236 (Vcc and VS are 5V)
isolator:VIL=0.5V, VOL=0.6 to 0.8V
TCA9511A:VIL=0.3*Vcc(1.5V), VOL=0.4V
INA236: VIL=0.4V, VOL=0.3V
Best regards