Part Number: MAX3243
Hello guys,
One of my customers is evaluatiing MAX3243 using own design PCB board.
When they checked DOUT VOH-IOH characteristics,
they found their MAX3243 capavility is lower than Figure 5-1 characteristics.
(it is less than 50%)
In that case, do you think what the cause is?
Is there any requirement to the capacitors? the maximin voltage? DC bias? temperature class?
Their Vcc voltage and ceramic capacitor values for charge pump are the follows?
VCC=5V,
Cbypass=0.1uF,
C1(located between C1+ and C1-)=0.1uF,
C2(located between C2+ and C2-)=0.47uF,
C3(located between V+ and GND)=0.47uF,
C4(located between V- and GND)=0.47uF
Your reply would be much appreciated.
Best regards,
Kazuya.