Part Number: DP83869HM
Dear TI expert,
Is there a maximum distance between the transformer and the DC83869 PHY? I have a multi-PCB design and need to separate them.
Thank you. Looking forward to your reply,
Jessica
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83869HM
Dear TI expert,
Is there a maximum distance between the transformer and the DC83869 PHY? I have a multi-PCB design and need to separate them.
Thank you. Looking forward to your reply,
Jessica
Hi Jessica,
Yes, we recommend 2" or less for the entire length of the MDI trace. This would include the trace between the PHY and the magnetics as well as the trace between the Magnetics and RJ-45. This is noted in our layout app note.
You may be able to get working communication with a longer MDI trace, however 2" is what we have known to give the most robust performance.
Best,
Shane