This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0303: No video from LMH0303

Part Number: LMH0302
Other Parts Discussed in Thread: LMH0303

Dear TI,

I have a design where I'm using GS12190 as HD-SDI cable driver and is working perfectly fine.

This circuit, I replaced with LMH0302 to get better SWaP. Here is the circuit 

 

I get no output from the circuit. Slew Rate is set to Low.. Reset is open , no register is set through SPI.

Do I need to set something through SPI? If yes, can I do without register settings via hardware changes?

I also tried adding 75R between C67 and GND on SDOn line.

Can you help in this?

 

Thanks 

Uday