Part Number: TUSB321AI
Other Parts Discussed in Thread: HD3SS3212, TUSB321
Hi,
Our design is:



Part Number: TUSB321AI
Other Parts Discussed in Thread: HD3SS3212, TUSB321
Hi,
Our design is:



Hello,
1. For TUSB321AIRWBR, the CC1, CC2 inside the chip and the CC1, CC2 on TYPE-C are staggered, rather than corresponding one-to-one:
For using the TUSB321AI with the HD3SS3212, CC1 and CC2 should be swapped per the typical application in the TUSB321AI datasheet:

2. The 900K on the VBUS_deT pin needs to be NC dropped, If 900k does not drop, the status of CC1, CC2, and DIR will be incorrect:
How is the TUSB321AI being used, as a DFP, UFP, or DRP?
If being used as a UFP or DRP, the VBUS_DET pin must be pulled up to VBUS with a 900KOhm resistor, or else TUSB321 will not be able to configure as a UFP.
Additionally, for a DFP application, please ensure that the ID pin is being used with a power switch or something similar to control when VBUS is being sent to the type-C connector. If VBUS is not controlled by the ID pin, the type-C connection will either work in only one orientation or will only work in USB2.
Thanks,
Ryan
Hello,
Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.
Thanks,
Ryan