Part Number: TCAN2857-Q1
Hello,
we want to use one HSS output controlled by the internal Timer On 20ms Cycle 2000ms.
A second HSS shall be used to be controlled by the Wake3/DIR input. On 300µs Cycle 50ms.
The VCC1 shall be active.
First question: Is this possible to control two HSS in sleep mode? One with Timer the second one with WAKE3/DIR?
According to Datasheet the sleep current for ISUPslpswodr is at 85°C typical at 60µA (see chapter 6.6 page 10)

How will the additional pulsed HSS will increase here the current. Acc. to Datasheet for ISUPhssnoload will increase the current typ. to 35µA. Is this only in active phase? So can I strip it down, if we are only active 20ms every 2000ms? --> 35µA x 20/2000 = 0,35µA?
![]()
Thank you for your support.
BR,
Martin