Part Number: DP83867CS
Other Parts Discussed in Thread: 66AK2L06, , DP83869
System information:
- SOC: 66AK2L06
- PHY: DP83867CS
- Diff pair impedance 100 ohms in PCPB
- 100nF series capacitors close to SGMII RX
- 100nF series capacitors close to PHY RX
Now our eye diagrams looks as follows, measured at SOC RX and immediately after the 100nF series caps and with full communication load:
We have observed that for close to 4 day continuous operation, about 50% of the boards have no rx align code errors. The other half we get one rx align error code per each hour of operation. Nothing deadly serious but we would like to tune the PHY SGMII TX to SOC to make this connection more robust.
Now we would like to tune the DP83867CS SGMII TX to SOC but according to datasheet there are no tuning values for slew rate, de-emphasis etc. Are there any hidden registers in PHY that would allow tuning?