Part Number: TUSB8043
Hello!
I am using TUSB8043 in my project. I need to change available configurations in OTP memory. Is there a tool that I can use for this?
Thank you in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8043
Hello!
I am using TUSB8043 in my project. I need to change available configurations in OTP memory. Is there a tool that I can use for this?
Thank you in advance!
Hi Artem:
Do you want to change configuration permanently or temporary just for experiment?
If for temporary , you can use SMbus mode with SMBUZ low to change internal register.
If for permanent, you can use external EEPROM with our EEPROM tool.
Regards
Brian
Thank you for response!
I need to set USB2_ONLY / REG_26h via OTP, because my board has no I2C EEPROM or SMBus master. Is there something like eFuse/OTP programming tool? May I ask you to provide me with it?
Best regards,
Artem
Hi Artem:
You can still use I2C master with SMBUSz pin low ( i2C address is 0x44 if pin 40 and 42 are low).
We do have efuse tool with USB connection to change internal register, but tool is for manual . For production, you still need to use EEPROM.
let me know which way you prefered, then I can send procedure.
Best
Brian
Thank you!
I will add EEPROM to design for next board revision. But now I need to make these changes manually on already mounted boards. So, may I ask you to provide me with efuse tool?
Best regards,
Artem
Please accept my friendship request , the request should be sent to your email.
Regards
Brian
Hello Brian,
I didn't receive a request on my email. May I ask you to repeat it?
Best regards,
Artem