Other Parts Discussed in Thread: TUSB1210, TUSB1211
I would like to clarify the VBUS, ID and REFCLK settings shown in Figures 10.1 and 10.2 in the TUSB1210 data sheet.
http://www.ti.com/lit/ds/symlink/tusb1210.pdf
In Figure 10-1 (Host or OTG, ULPI Input Clock Mode Application Diagram) a USB Type B (device) connector is used. There is a VBUS Switch to apply power to this Type B connector. Further, the ID pin of the Type B connector is tied to the TUSB1210. The section title and wording suggests this section is intended for a Host application, yet the Type B connector and the ID pin suggest a Device mode application. Finally, the REFCLK is tied low in this configuration.
The converse is shown in Figure 10-2 (Device, ULPI Output Clock Mode Application Diagram) for a Device Mode application.
Can you please confirm the correct implementation?