Hi,
I am designing a LED video display board which uses three LVDS pairs for data distribution (clk + 2 data channels).
Clock rate is 60Mhz, with data on both edges. Using the two data channels the total data rate is 240Mbit/s.
From a data point of view, it is a multidrop bus, where each pcb sees the same data.
The LED panels are 340 mm wide (FR4 material), and data goes in on left side and goes out on the right side,
and will be "daisy chained" with up to 10 boards in row. This means the signals goes through 3.4 meters of FR4 pcb.
I will repeat the LVDS signals on each board.
I am worried about added clock jitter and skew so the margins will become smaller and smaller towards the
end of each LED panel row.
Is it a good or bad idea to have LVDS repeater/buffer on each pcb ?
The options I have:
1. Using a quad LVDS buffer like DS15BR400TSQ on each pcb (adding very litter skew and jitter I Believe) and
then locally drop the signals on each pcb from the bus with a DS90LV032A (placed close to the outputs of the buffer).
2. Translate to single ended with LV032 and then "retransmit" with a LV031 towards next board?
3. Only buffer LVDS signals on, lets say, every 4:th pcb.
I suppose the speed is fairly low in LVDS terms, but adding jitter/skew from 10 pcb boards would reduce the margins.
Anyone with experience of a similar LVDS configuration ?
What could I expect from a configuration like this ?
Would be great if I could use higher data rates as well (100Mhz maybe).
What LVDS devices should I use.
Kind regards
T