This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

max3238e, max3243e, max3221e



Scenario: VCC remains applied to all transceivers.

R-OUT1,2,3 (ie,not R-OUT1b) from 2 (or multiple) transceivers connected together when FORCEOFF = L  on all the transceivers except the 1 active transceiver.

Can D-OUTS from 2 (or multiple) transceivers be connected together when FORCEOFF = L  on all the transceivers except the 1 active transceiver.

Is the D-OUT = Z capable of withstanding an impressed RS-232 voltage ?

  • Charlie,

    Normal ROUT pins can be connected together when ~FORCEOFF is low (or ~EN is high if applicable to device) because the ROUT pins will be high impedance output.

    DOUT pins can be connected together when ~FORCEOFF is low because the DOUT pins will be high impedance output (over a +/-13.2V range).