Other Parts Discussed in Thread: DS90CR287
Hello,
I have a question about the input clock of the DS90CR287 Channel Link transmitter:
The datasheet clarifies that the input clock must be valid when powering up the device.
Do I also have to use the PWR_DOWN pin if I want to change the frequency of the transmit clock during operation?
It's no problem for my application if the transmitted data would be invalid for some time, until the PLL locks to the new frequency (TPLLS <= 10ms).
Thanks,
Ralf