We have a requirement to pass the LMH0030 output signal from the middle of a long, thin board to the buffer chip (LMH0002) at the end. Space constraints require this signal to be routed on an inner layer of our FR4 PCB & we are really struggling to find a geometry to give 150 Ohms differential impedance. The LMH0030 datasheet gives dire warnings about driving 50 Ohm loads, yet SNLA196 ("LMH003x FAQs") suggests a method with 100R differential traces. Our board house is suggesting a geometry which will give 138R. Can we work with this? What should the LMH0030 load resistors be? At the moment they are placed at the drive end of the transmission line with the termination resistor across the buffer inputs.