This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD rating of ESD protection devices

Other Parts Discussed in Thread: TPD2E009

Hello TI and fellow community members,

looking for an ESD protection device with low capacitance I came across parts like the TPD2E009. The datasheet claims compliance with IEC61000-4-2 Level 4. The absolute maximum ratings specify, however, a limit of 8kV for air discharge events. According to IEC Level 4 it should withstand at least 15kV. What is the reason for this discrepancy?

Best regards,
Sebastian Winter