This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2003 - Confirming Vce(sat) and Ii over Temperature

Other Parts Discussed in Thread: ULN2003A, TPL7407L, SN65472-EP, SN75477, SN75472, DRV8803

We have an application where we will use the ULN2003A to drive a fairly resistive output from +28V to GND. The input voltage will be 0 to +3.3V.

I want to confirm that I am correctly reading the datasheet and that for a load (sink) current of approximately 20mA (50mA max), each output will have a maximum Vce(sat) of approximately +1.2V over the operating temperature range (-40C to +105C); with +1V being a typical value (over temp).

I also want to confirm that each input will have a maximum input current of approximately 1.2mA over the operating temperature range (-40C to +105C); with 700uA being a typical value (over temp).

Thanks in advanced.