Other Parts Discussed in Thread: TUSB8041-Q1
Hi
I am in an early stage of designing a USB 3.0 hub. I was thinking of using tusb8041-q1 automotive grade for design as my product have a fair share of automotive market. I have couple of qustions
1. What is this automotive grade different from the catalog grade? I am seeing there is a package difference and price?
2. Can I use the same reference design as shown in url: http://www.ti.com/tool/tida-00288
3. My hub would be connect to a host pc with USB 3.0 port. But the downstream ports would be two usb 3.0 device and two usb 2.0 device(as shown in attachment). Data rate is very critical in my application. I want 5GbPS from USB 3.0 devices and 480mbps from USB2 devices simultaneously. In other-wards, the plugging in of usb 2.0 devices should not downgrade the hub performance to usb 2.0. Is it possible?