Other Parts Discussed in Thread: DS36277, SN65HVD1785, SN65LBC184
Gentlemen, I hope you can provide me an educated advise on the following:
I am currently working in the design of a telematic system to remotely perform a number of simple actions on a vehicle. To make things easier and not get into a CAN or LIN interface, I would like to implement a low speed serial bus (physical layer of SAE J-1708 standard, used under a custom simple protocol of my own) to communicate my main control module with the remote actuators. It will be fine working at 9.6 kbps, as stablished in J-1708, so a super high speed is not required on the transceiver.
Being common in an automotive electrical environment heavy transients, etc, what set up would you consider robust enough for this?
My initial approach includes the DS36277 choice, protected on the outside by two MOVs, two TBUs and a dual TVS, as shown on TI literature.
Thanks in advance for your comments,
Norb.