This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS171 - Internal circuit of 3 level input pins

Guru 19785 points

Other Parts Discussed in Thread: TMDS171

Hello Team,

Could you please share us the internal circuit of the 3 level input pins of TMDS171 (PRE_SEL, EQ_SEL/A0, TX_TERM_CTL, SWAP/POL pins) ?

When you float this pin and monitor the pin voltage, DMM showed 0.9V which is out of the Vim range. Instead of floating the pins and used 65kOhm pull up/down resistors like in the application schematic in the datasheet, DMM showed 1.4V. This is the maximum value of the recommended range. We would like to know how to set the pin voltage to the middle of the Vim.

Best Regards,

Kawai