This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983A with TPS65982, HARD RESET occur when TPS65982 sends DR swap

Other Parts Discussed in Thread: TPS65982, TPS6598X-CONFIG

Hi Team,

One issue with TPS65983 and TPS65982

The TPS65982 is with 1.7.6 FW and TPS65983 with 3.3 FW

TPS65982 FW as DRP and enable initial swap to DFP

TPS65983 use Apex Creek FW

Follow below sequence, then we see HARD RESET

1. TPS65982 power up with VIN_3V3 = 3.3V and PP_5V0/PP_CABLE = 5V

2. Plug in TPS65983 board(apex creek), then TPS65982 is DFP and sink

3. Turn off TPS65982 VIN_3V3 and PP_5V0/PP_CABLE power

4. see the connection loss and re-establish, TPS65982 will then send data role swap to be DFP

5. HARD RESET occur after the DR SWAP command

Below is the trace record after turn off TPS65982 VIN_3V3 and PP_5V0/PP_CABLE, then see HARD RESET after DR SWAP

If we change TPS65983 board to TPS65982 with Apex creek FW, then no see HARD RESET 

Could you help check? Thanks!

T303_S3_pluged in to Apex creek_983A.usb

Sam