Other Parts Discussed in Thread: TRS3232E-Q1
Hello,
I'm concerned about how TRS3232E-Q1 will withstand a negative voltage which could be applied to its VCC pin. In the system, -32 V could be applied to the VCC pin, but a resistor of 2.2 kΩ will be put on the VCC line to prevent an excessive current flown out of the VCC pin. A Schottky diode of about 0.35 V will also be added externally to the VCC pin, therefore the negative voltage will be clamped to nearly -0.35 V at the VCC pin.
- Does TRS3232E-Q1's VCC pin have an internal clamping diode against a negative voltage? I guess the data sheet's Absolute Max Rating of VCC -0.3 V to 6 V suggests the existence of a diode inside the chip.
- If the above is correct, a current of about 14.4 mA could be flown out of the VCC pin when -32 V is applied through the 2.2-kΩ resistor. Could the device survive or damage?
Best regards,
Shinichi Yokota