Part Number: TUSB321
Other Parts Discussed in Thread: TUSB542
Hi !
I am using TUSB321 along with TUSB542.
TUSB321 is used to detect cable inversion and appropriately switch the TUSB542 mux.
I am observing some instability in cable inversion detection. This is not consistently working. This is used in UFP mode, where port pin is pulled down.
Using 909K pull on VBUS_DET. The datasheet says there is a 95K pull down on the pin. If we use 909K, the voltage at VBUS_DET settles around 0.4V . This conflicts with the datasheet where the VBUS_DET threshold is 2.95 to 3.8V.
If I put 47K instead of 909K, the voltage settles around 3.2V. Even after changing to 47K, the CC logic still fails to detect.
Did anyone see this issue or comment on what could be wrong.
Regards
Abdu Samad