Part Number: TPS65982-EVM
I have several TPS65982-EVM (Rev 1.0) that when running the originally supplied (factory) firmware work as expected in configuration ID 12 (Mid Power Charger Adaptor).
If I try to either recover after software experiments, or just update using TPS6598x Application Customizer 2.12, Configuration 12 no longer works.
Using an Aardvark, I can load directly from TPS6598x Application Customizer 2.12, Device/Reflash EVM Firmware (Recovery). The firmware loads and verifies.
Or, I can use the Aardvark FlashCenter and the EVM recovery binary supplied with 2.12, and the firmware loads and verifies.
In both cases, Configuration ID12 no longer functions. By that I mean, the power LED is ON, but when connected to a Dell tablet, instead of lighting the 5V LED and PVDR LED as expected, it only lights the CONS LED, and no current flows in the Vbus, although the EVM is powering the Vbus at 5 Volts.
Is there something else I need to do to recover these modules? Such as reload a different version Low Region Binary to go with the firmware?
Is there a way to find out what version firmware is loaded on an EVM?