Hi,
I'm using the and TSC2017EVM and USB-MODEVM Interface (TSC2017EVM-PDK). Normally the USB interface should be connected to a PC via a USB cable.
But, I would like to put my PC far from my USB-MODEVM Interface (20m). And I also need 2 modules be electrical isolated. So I'm thinking to use the optical fibre and two modules to convert USB to Fibre optic and Fiber Optic to USB.
Do you have any advice/command or device to suggest?
Thanks,
Leila