Other Parts Discussed in Thread: DS90LV017A, SN65LVDS2, DS90LV018A,
We have 2 circuit boards that need to communicate over an external LVDS cabled interface. The interface is a basically a master/slave SPI bus using the LVDS drivers/receivers for the 'cables' part of the interface. One of the boards uses the DS90LV017A/DS90LV018A devices and the other board uses SN65LVDS1/SN65LVDS2 devices.
In certain circumstances, all of the DS90LV017A/DS90LV018A components on the 'master' board will get blown. In the blown condition, the devices get very hot in circuit, removing them from the board I find that the VCC pin is shorted to GND at about 10 ohms.
The boards are each separating powered and can be powered up in any order. Is there some sort of latch-up condition occurring?