This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TUSB9261: TRIM support in BOT mode

Part Number: TUSB9261

Tool/software: Linux

Hi,


we are operating an mSATA device behind a TUSB9261 (v1.05) under Linux 3.14 with ext4. The usb-storage driver tells us that the WRITE SAME SCSI command is not supported by the device.

There is still the UNMAP SCSI command which could activate TRIM. However, does the TUSB firmware translate this command into the TRIM ATA command and provide support for that?

Are there any other ideas how to trigger TRIM in BOT mode?

Thanks for every hint!