Part Number: TUSB1310A
Other Parts Discussed in Thread: TUSB1310
Hi USB Team,
My customer has a couple questions on the TUSB1310A, they are only using the SuperSpeed operation and not using the USB2 PHY.
1. For TUSB1310A external clock: which input is recommended for the best Tx and Rx jitter performance:
a. XI (A12) as single-ended 1.8V clock input ?
b. REFCLKP/REFCLKN (C13/C14) as differential clock input ? These pins are marked reserved in TUSB1310A datasheet but shown in the SuperPHY and Ultrahub schematics for old TUSB1310.
2. We are revising the TUSB1310A power supply filtering and decoupling to bullet-proof the Tx and Rx jitter performance and would like to know some more info on certain pins. Please confirm/answer the following ?
a. Pin P12 VDDA3P3 appears to be ONLY used for USB2, is this correct ? If so we will not focus on its filtering/decoupling.
b. Pin C10 VDDA1P8 in the Ultrahub schematic is named US3_VDDO_1P8 and has optional connection to digital 1.8V. What I/O does this pin provide power to and are we better off leaving it separated from sensitive 1.8V analog power ?
c. Pin C11 VDDA1P1 in the Ultrahub schematic is US3_VDDO_1P1. Which I/O does this pin provide power to and are we better off leaving it separated from sensitive 1.1V analog power ?
Please let me know if you have any questions.
Thank you!
Regards,
~John