Other Parts Discussed in Thread: TUSB320
I am designing a product that will implement a USB C receptacle. My requirements are below:
- Powered by USB Bus (5V) from USB C receptacle
- Needs to handle 3A of current
- Needs to support either USB 2.0, 3.0, or 3.1 USB protocols to communicate with the device
- Different types of cables can be plugged into the device from a PC (A to C, C to C, etc)
I am still learning about USB C protocol and the power delivery specs. From what I can see from the TPS25741 device, this should be able to handle the specs that I need. My major concern is regarding the USB A to C cable from a PC. If I plug in a USB A to C cable from a USB 2.0 port on a PC into this device, will it be able to handle 3A of current?