Other Parts Discussed in Thread: SN74AVC4T245, , SN65LVDS2
Hi,
In my design SN74AVC4T245 is used to level shift 1.8V clock to 3.3V.
I have to convert differential clock from ADC to single ended and single ended clock from SoC to differential for DAC.
1) Can I connect the output of SN74AVC4T245 to SN65LVDS1?
2) Can I connect output of SN65LVDS2 to SN74AVC4T245?
3) Will the SN65LVDS1 support CMOS level?
4) Is there any other single ended to differential converter from TI which has zero delay?
Regards,
Shanu V