Part Number: DS90UB964-Q1
Hi,
I would like to confirm that one of I2C slave device (serializer) is busy at broadcasting of UB964.
Can the UB964 confirm which slave device is busy?
Also, the UB964 is busy?
Regards,
Kenshow
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB964-Q1
Hi,
I would like to confirm that one of I2C slave device (serializer) is busy at broadcasting of UB964.
Can the UB964 confirm which slave device is busy?
Also, the UB964 is busy?
Regards,
Kenshow
Hi Kenshow,
When UB964 is in broadcast mode, it cannot distinguish ACKs from the remote slaves as all slave device have been assigned the same aliases ( a requirement for broadcasting a command). ACK is an OR operator of the responding remote slaves via I2C.
I suggest reviewing the following thread: 
Regards,
Davor
Hi Kenshow,
Yes, each FPD-Link III device features an I2C interface that can perform a function of a I2C master capable of arbitration with other masters, allowing multiple masters and slaves to exist on the same I2C bus.
Regards,
Davor
Hi Kenshow,
The '964 does not have a way of knowing if one of the remote slaves is busy in broadcast mode. Once it receives an ACK from one of the slaves, it will be ready to broadcast another command.
Regards,
Davor
p.s. I will be out of office until 7/31.