Part Number: DS32EV400
Hello! I have been searching for an IC for the purpose of extending a DisplayPort cable length to up to 20 meters for driving one Full HD monitor. I plan on putting the device in the middle of the cable to re-condition the signal. According to my research so far, the simplest solution appears to be the DS32EV400, Quad Equalizer (http://www.ti.com/lit/ds/symlink/ds32ev400.pdf).
This equalizer clears out the intersymbol-interference of the 4 DisplayPort main-links, and then boost the signals with a limiting amplifier. According to page 13, I should pull all BST_N to high if I am to place the device at 10 meters.
1) Is this IC is suitable for my application (cable extension)?
2) Other than ISI and voltage drop that this chip presumably can deal with, there might also random jitter and phase distortion. In my knowledge, equalizer cannot deal with them. Should I be concerned?
3) It appears that AUX and HPD are left untouched. I believe HPD is just a discrete signal, so that's okay. But can the AUX signal travel for 20 meters without equalizing and boosting?
4) Are there any other IC that I should be looking into? The design will not be able to support I2C.
Thank you for your help!