Part Number: TDP158
Dear Sir,
Can we leave HPD_SNK, SCL_SNK and SDA_SNK pins unconnected when not used ?
External device is implemented with L/S integrated and ESD protection and so no need for these pins.
thanks
Paul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDP158
Dear Sir,
Can we leave HPD_SNK, SCL_SNK and SDA_SNK pins unconnected when not used ?
External device is implemented with L/S integrated and ESD protection and so no need for these pins.
thanks
Paul
Hi Paul,
When the device is connected in snoop mode (HPD_SNK, SCL_SNK/SDA_SNK are connected, HPD_SRC is floated, and SCL_SRC/SDA_SRC are tied to GND), you don't need extra configuration, please use snoop mode.
If you don't want to use HPD and DDC at all, you can leave HPD_SNK and HPD_SRC floated, SCL_SRC/SDA_SRC are tied to GND and SCL_SNK/SDA_SNK connected to 5V with 2k pull-ups. Then you will have to: disable HPD automatic power down(0x09[2]) and
Disable HPD automatic power down(0x09[2])
Disable DDC training (0x0B[0])
Set the right mode of operation HDMI1.4 o HDMI2.0(0x00B[1]) this will change when the data rate changes
Using snoop mode is the best choice.
Regards