This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982-EVM: Reference design for USB Type-C PD sink with USB 3.0 Superspeed data?

Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982, HD3SS460

Do you have a complete reference design for a USB Type-C PD sink that passes USB data and superspeed signals to a Type A connector or pin header?

We want to verify our USB 3.0 device with a PD sink of 15V-20V @ 2A works with various laptop hosts / PD sources.

We just finished testing the TPS65982-EVM with several USB Type C PD sources and are satisfied with the PD profile negotiation. 

If there is no such PD + superspeed data eval board or design available, do you recommend we develop with the TPS65982 or a different TI USB Type C PD controller?

Thanks!!

Jason