Part Number: TPS25740A
Other Parts Discussed in Thread: TPS25740B, TPS25741A
Team,
My customer is working on a project using our TPS25740A, and has a few questions:
I’m testing with the TPS25740A, and I think I’m seeing a violation according to the datasheet. It appears that the TPS25740A is registering a SUVP (Slow Under-Voltage Protection) fault after the IC has switched in the additional SMPS feedback resistors. The datasheet says that during voltage transitions, the SUVP is disabled.
In the attached photo:
- Blue = SMPS output
- Yellow = VBUS switched output controlled by the TPS25740A
- Green = CTRL1 or CTRL2 … pulled to GND is when the voltage is supposed to start transitioning
I also have an issue in the SMPS that it gets a spike at the beginning of the transition, stops regulating, then the VBUS voltage droops. You can see where it crosses the SUVP limit and VBUS is turned OFF.
Another aspect to this issue is that this happens when I load the PD Device with a 0.1A resistive load. If I remove that load, everything transitions correctly. There is still a dip in the SMPS output, but it is much smaller and doesn’t appear to activate the SUVP fault.
I would love to find out that this is an error in the TPS25740A die that was corrected in the TPS25740B! I need to apply some “fixes” to my board, then I can repeat this testing on the “B” version.
Thanks
Viktorija