Part Number: ISO5851
Tool/software: WEBENCH® Design Tools
Dear SIrs!
We used the Semikron IGBT - Semix604GB12 type. It has (contains) 4 IGBT with separated 4 gate drives G_E connections - and we used distributed drive resistors(2/3*R at Gate and 1/3*R at emitter) to all IGBTs.
We would like to use the mentioned IGBT in parallel connection.
We staded your reference design - TIDUC70a with the ISO5851 driver.
Do you have a suggestion or a study - how can we modify the circuit - how is it able to drive the 2*4 ->8 pcs. IGBT?
Best regards: Jenő csizmazia