Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB542, TUSB321,
Our current design uses a TUSB542 and we failed USB 3.0 for current in U3. TUSB542 continues to draw active current for ~300 ms after a GoToU3 (TD 4.10.3 of USB_Type_C test spec).
We plan to use the HD3SS3220 in place of the TUSB542+TUSB321; the HD3SS3220 does not discuss U2/U3 or any low power mode and I assume that this is because its active current is already low. My understanding from the datasheet is that the supply current, ICC, never exceeds 900 uA, under any condition, is that correct?
What is the reason that these two muxes have such a large difference in power consumption? Is there some other performance advantage of the TUSB542+TUSB321? I don't want to change the design to find out we fail for some new issue related to the device.